Showing and Hiding Perspective Components - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Procedure

  1. In the left pane of the Perspective Management dialog box, select the component you want to show or hide.
    Note: You cannot select a perspective frame or container at the root level to show or hide.
  2. In the right-pane, select the Visible check box to show the component, or clear the Visible check box to hide the component. If the component also has nested subcomponents, these are automatically shown or hidden based upon the choices you made for the parent component.
  3. Click Apply.
  4. Click Close.