Widgets are items that display specific information and include specific functional behaviors. The Classic View perspective includes all of the following widgets, except for the System Selection Information widget.
Note: The Advanced Data, BACnet Exposed, Connections, Local Display, Logic View, Parameters, State Tables, and System Selection Information widgets are known as specialized widgets because they have no configurable data.
Icon | Section | Property Selection |
---|---|---|
Specialized widget that allows you to view and work with advanced controller information. See Advanced Data widget. |
Visible |
|
Specialized widget that allows you to view and work with points in the application. See BACnet Exposed widget. |
Visible |
|
Specialized widget that allows you to view and work with connections of the Control Sequence. See Connections widget. |
Visible |
|
Configurable widget that allows you to view the details of a BACoid (BACnet Object ID). See Details Data widget and Data Criteria. |
Data Criteria Type Visible |
|
Specialized widget that allows you to view and configure the display device. See Display widget. |
Visible |
|
Specialized widget that allows you to view and work with application logic. See Logic View widget. |
Visible |
|
Specialized widget that allows you to view parameters. See Parameters widget. |
Visible |
|
Specialized widget that allows you to view and work with State Table information. See State Tables widget. |
Visible |
|
Specialized widget that allows you to view system design information. See System Selection Information widget. |
Visible |
|
Configurable widget that allows you to select and display multiple BACoids using data criteria. See Table Data widget and Data Criteria. |
Data Criteria Type Visible Order |