Simple View Components - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table shows how the Simple View is broken into components of a perspective.

Table 1. Description of Simple View as Perspective Components
Simple View Component Type Orientation/ Location/ Data Criteria Direct Subcomponents Appearance Description
Entire Simple View Tab Container Top

Orientation Container (Application)

System Selection Information Widget (System Selection Information tab)

The Simple View is a tab container that specifies that the two subcomponents appear as tabs.
Application Tab Orientation Container Horizontal

Table Data Widget - UI Column (Inputs column)

Parameters Widget (Parameters column)

Table Data Widget - UI Column (Outputs column)

The orientation container type specifies that the three subcomponents be arranged horizontally, or stacked next to each other.
Inputs Table Data Widget UI Column None The Table Data widget with UI Column data criteria specifies that Miscellaneous Inputs, Network Inputs, and Sensors appear within the same table in the UI.
Parameters Parameters Widget Not Applicable None The parameters widget displays application parameters and cannot be configured.
Outputs Table Data Widget UI Column None The Table Data widget with UI Column data criteria specifies that Control Points, Miscellaneous Outputs, and Network Outputs appear within the same table in the UI.
System Selection Information Tab System Selection Information Widget Not Applicable None The System Selection Information widget displays system selection choices and cannot be configured.