Container - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
When you build a perspective, containers allow you to organize the content according to specific properties. Container types include Frame, Orientation, and Tab. Each container type can be added individually. In addition, after adding a container, you can change the type to another type of container, such as switching an Orientation container to a Tab container.

Table 1. Container Types and Properties
Icon Description Properties
Indicates a Frame container, which can only be added at the root level.

Orientation

Indicates an Orientation container, which can be vertical or horizontal.

Orientation

Resizable

Visible

Indicates a Tab container, which can be positioned in various locations of the UI.

Position

Visible