Viewing and Adding Unmapped Objects - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
About this task

Certain objects are not always exposed within the CCT/PCT UI. To expose the objects for viewing, follow these steps:

Procedure

  1. In the CCT/PCT UI, right-click the output controller and select Logic View. The Logic View appears.
  2. Select Control Mode. This view shows the flow of the PID.
  3. Right-click the PID and select Expose Ports > For BACnet. See Figure 1.
    Figure 1. Expose Ports for BACnet

  4. To map objects, see Adding Objects Manually or Adding Objects Using Auto-Discovery.