Attributes (Last Value) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The following table describes the attributes used by the Output Controller Last Value (Boolean, Enum, Float) modules:

Table 1. Last Value (Boolean, Enum, Float) Attributes

Name

Type 1

Description

Default Value

Input

 

Contains a Default Value of this Input that is passed to the Present Value on the first execution after startup or enable. Otherwise, the Current Value of the Input is passed to the Present Value.

False

1st Enum0.0

Present Value

G, V

Contains the output of this module

 
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)