Primary States (Sideloop Reset Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Min: The Present Value is set to Output Range Low.

  • Max: The Present Value is set to Output Range High.

  • Control: The Input is spanned using the Input Range Low, Input Range High, Output Range Low, and Output Range High to produce the Present Value.