Reliability (Sideloop PI With Reset Staged Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Sideloop PI With Reset Staged Output Reliability

Input

Behavior When Input Is Not Reliable

Process Variable

If the State is Control, the PID skips execution and holds its output at its last value.

Reset Input

The last Reliable value is used as the input.