Attributes (Sideloop Interlock Binary to Binary) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Sideloop Interlock Binary to Binary module.

Table 1. Sideloop Interlock Binary to Binary Attributes

Name

Type 1

Description

Default Value

Input

 

Contains input to this module.

Off

Set Name: Off/On

Mode

 

Contains the connection to the Selection object of a control System. It overrides the internal logic.

Control

Set Name: Off/On/Control

Present Value

G, V

Contains the output based on the input and the status of the associated delays.

Set Name: Off/On

SL-DELAYTYPE (Delay Type)

 

Selects the type of delay from the time the binary input is energized or de-energized to the time when the analog output goes to Output Range High or Output Range Low. This can be set to None, On, Off, or Both.

None

Set Name: BI to BO/AO Delay Type

SL-OFFDELAY (Off Delay)

 

Selects the delay from the time the input is de-energized to the analog output going to the Output Range Low.

30 Seconds

SL-ONDELAY (On Delay)

 

Selects the delay from time the binary input is energized to time when the analog output goes to Output Range High

30 Seconds

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)