Primary States (Zone Damper w Staged Heating) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The key states are described below. If the Heating Mode is Shutdown, the Heating Percent Cmd is set to 0%, and the state is not allowed to enter Control Heating. Otherwise, the Cooling Mode is Control and the Zone Temperature is reliable. A two-state FSM determines whether heating or cooling should be active.

Cooling Mode

  • Control: Modulates the zone damper to control the Process Variable at the Effective Setpoint. If the Process Variable is unreliable, the Damper Percent Cmd is set is based on the Unreliable output input.

  • Shutdown: Sets the Damper Percent Cmd based on the Shutdown Option input. If the input PID Tuning Reset is Normal, the Reset Tuning input to the PID is set to true causing the PID to recalculate its tuning parameters.

Heating Mode

  • Control: Cycles the staged heating to control the Process Variable at the Effective Setpoint. If the Process Variable is unreliable, the Heating Percent Cmd is set based on the Unreliable Option input. If the input PID Tuning Reset is not Normal, the Reset Tuning input to the PID is set to true causing the PID to recalculate its tuning parameters.

  • Shutdown: Sets the Heating Percent Cmd based on the Shutdown Option input.

Table 1. Zone Damper w Staged Heating Command Hierarchy

Cooling Mode

Heating Mode

Shutdown Option

Unreliable Option

ZN-T Reliable

FSM State

PID Tuning Reset

State

Hold

       

*

Reset 1st PID

 

Hold

         

Reset 2nd PID

 

Hold

         

*

 

*

Hold

       

Reset 1st PID

 

*

Hold

       

Reset 2nd PID

 

*

Hold

       

*

 

Shutdown

Not (Control)

Open (Cooling)

*

*

*

 

Open (Cooling)

Close (Heating)

*

*

*

 

Close (Heating)

Hold Damper

*

*

*

 

Hold Damper

Control

*

*

TRUE

*

 

Control Heating

Open (Cooling)

FALSE

*

 

Open (Cooling)

Close (Heating)

*

 

Close (Heating)

Hold Damper

*

 

Hold Damper

Not (Shutdown)

*

*

*

TRUE

Cooling

 

Control Cooling

Heating

 

Control Heating

Open (Cooling)

FALSE

*

 

Open (Cooling)

Close (Heating)

*

 

Close (Heating)

Hold Damper

*

 

Hold Damper