Reliability (Lighting) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following reliability states only apply when Feedback Provided = True. Otherwise, the last reliable input values are used.

  • Reliability is set to Failed to Synchronize if LC is unable to make the Light Status reflect the desired Present Value (after 1 minute delay - 30 seconds before changing the Polarity output and another 30 seconds waiting for synchronization).

  • Reliability returns to Reliable from Failed to Synchronize if the Light Status changes at a later time (without the Present Value changing) so that it now matches the desired Present Value.

  • Reliability changes to Failed to Synchronize if Light Status changes so that it no longer matches the desired Present Value.