Attributes (Lighting) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Lighting Control modules.

Table 1. Lighting Attributes

Name

Type 1

Description

Default Value

Feedback Provided

C

Indicates whether the lighting hardware provides binary feedback indicating the actual status of the lights. The Lighting module’s Feedback Provided input should be set True only for the Pulsed BO with BI Status hardware type.

False

Input

 

Contains the desired state of the lights. If the Input is unreliable, the last reliable value is used.

Off

Set Name: Off/On

Light Status

 

Status of the lights from pulse-type lighting control hardware.

Off

Set Name: Off/On

LIGHT-DELAY (Light Shutoff Delay)

 

Specifies the time between the warning blink (if issued) and the light being permanently switched off. If the Lighting module’s Lighting Operating State is Waiting to Shut Off and the Light Shutoff Delay is changed, the current time remaining is discarded and the Lighting module starts a new timer for the new Light Shutoff Delay.

120 Seconds

Lighting Operating State

V

Current state of operation for the module.

Lights Off

Set Name: Lighting Operation

LIGHT-WARN (Warn Occupant)

 

Indicates that the Lighting module should issue a warning blink before the lights are permanently switched off.

True

Polarity

V

Output used to synchronize pulsed-type lighting output devices (Feedback Provided = True) so that the Light Status matches the Present Value. If Feedback Provided = False, the value for the Polarity output always remains Normal. The Lighting module assumes that changing the Polarity causes the Binary Output object to issue an extra pulse. If the Binary Output used does not support this behavior, the user must connect the Present Value and Polarity outputs to the inputs of an XOR block and connect the output of the XOR block to the Binary Output.

Normal

Set Name: Polarity

Present Value

G, V

Current output of the module.

Set Name: Off/On

Sync State

V

Current state of the synchronization of the pulse-type lighting control hardware.

Present Value Changed

Set Name: Lighting Sync State

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)