-
Off: Set Humidity Percent Cmd to 0% and turn off all the stages, but observe the minimum on and off timers. If this state is active longer than the Basin Delay Time and Basin Drain Enable is True, the drain valve opens and the fill valve closes.
-
Instant Shutdown: Turn everything off and do not observe minimum on and off timers. Close the fill valve and open the basin drain valve.
-
Hold: Holds the outputs at their current position. If the Output Overridden is true, then the Output Position input is passed to the Valve Percent Command.
-
H Control: When operating in the H Control mode, the module controls the process variable (either return humidity or zone humidity) to the setpoint. As the humidity drops below the setpoint, the analog percent output Humidity Percent Cmd increases, which with the intervention of the MSC module causes the controlled devices to remain on longer and/or turn on more devices. The fill valve opens and the drain valve closes. The pump stays off for an adjustable amount of time (Basin Fill Time) to allow the basin to fill if the drain valve was open when this state first occurred.
-
Limited H Control: When operating in the Limited H Control mode, the module controls the discharge humidity to the setpoint. As the humidity rises above the setpoint, the analog percent output Humidity Percent Cmd decreases, which with the intervention of the MSC module causes the controlled devices to remain on less time and/or turn off more devices. This mode is the humidity high limit mode and is intended to prevent the discharge air from becoming too humid. The fill valve opens and the drain valve closes.
Mode |
PID Tuning Reset |
State |
---|---|---|
Off |
* |
Off |
Instant Shutdown |
* |
Instant Shutdown |
H Control |
* |
H Control |
Limited H Control |
* |
Limited H Control |
Hold |
Reset 1st PID |
Limited H Control |
Hold |
* |
Hold |
Drain Basin |
Mode |
State |
---|---|---|
True |
* |
Instant Shutdown |
False |
Off |
Off |
False |
Instant Shutdown |
Instant Shutdown |
False |
H Control |
H Control |
False |
Limited H Control |
H Control |
False |
Hold |
Hold |
Drain Basin |
Mode |
State |
---|---|---|
True |
* |
No Limit Control |
False |
Off |
No Limit Control |
False |
Instant Shutdown |
No Limit Control |
False |
H Control |
No Limit Control |
False |
Limited H Control |
Limited H Control |
False |
Hold |
Hold |