Module Use in Applications (Humidification Proportional Steam Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Humidification Proportional Steam Output Uses in Application System Selection Trees

Module Instance Name

Applications

Proportional Steam Humidification Control v51

All Air Handling Unit Applications

To see a module's connections and how modules interact with it, view the Connections table.