Attributes (Humidification Proportional Steam Output) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Humidification Proportional Steam Output modules.

Table 1. Humidification Proportional Steam Output Attributes

Name

Type 1

Description

Default Value

Compensator Humidity Cmd

 

Controls the humidifier valve. The valve is commanded from 0% to 100%. This output incorporates the Lead Compensator.

0.0

Display Units: %

Delay

 

Defines the time that the Humidity Percent Cmd is held at 0% following activation of the Isolation Valve Command.

300 Seconds

Discharge Humidity

 

Contains the process variable when the activity operates in the Limited H Control mode.

70.0% RH

Discharge Humidity Setpoint

 

Contains the desired process variable setpoint when the activity operates in the Limited H Control mode.

70.0% RH

Humidity Control Status

V

Contains the current saturation status of the controller.

Set Name: Control Status

Humidity Percent Cmd

V

Contains a representative analog percent output on a scale of 0% to 100%. This output should be connected to the humidification control device.

Display Units: %

Humidity Process ID

 

Defines the type of process being controlled. This input must be set to either zone humidity or return humidity depending on the actual process.

RA-H

Set Name: Process ID

Humidity Process Variable

 

Used for either the return air humidity or the zone air humidity. This is the process variable when the activity operates in the H Control mode.

40.0% RH

Humidity Setpoint

 

Desired process variable setpoint when the activity operates in the H Control mode.

40.0% RH

HUM-OUTSTATE (State)

G, V

Contains the current operational mode of the output controller.

Set Name: AHU Hum Prop

Isolation Valve Command

V

Enables the steam isolation and/or humidifier jacket valve when controlling a proportional steam humidification valve. This output would be ON anytime humidification is required.

Set Name: Off/On

Mode

 

Mode requested by State Selection.

Off

Set Name: AHU Hum Prop

Output Overridden

 

Indicates when the actual output controlled by this output is overridden by a user.

False

Output Position

 

Provides the current Present Value of the output that this controller drives.

0%

PID Tuning Reset

 

Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID.

Normal

Set Name: PID Tuning Reset

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)