The following table describes the attributes used by the Heating Staged Outputs with Low Limit modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Control Band |
V |
Control band for the MSC. |
Display Units: °C, °F |
Eff Minimum Off Time |
V |
Minimum off time to be used by the MSC. |
Display Units: Seconds |
Eff Minimum On Time |
V |
Minimum on time to be used by the MSC. |
Display Units: Seconds |
Eff Process Time Const |
V |
Contains the effective process time constant that is used by the MSC. |
Display Units: Seconds |
Eff Process Variable |
V |
Contains the Process Variable to be used by the MSC. |
Display Units: °C, °F |
Heating Control Status |
V |
Current saturation status of the controller. |
Set Name: Control Status |
Heating Ramp Rate |
Determines the time to remain in the Cold Start state (if applicable). During the cold start state, the preheat output is prevented from closing quickly to allow it to come into control without tripping the Low Limit on the unit. |
20 Change per Minute |
|
HTG-MINOFF, PH-MINOFF, or RH-MINOFF (Minimum Off Time) |
Contains the Min Off Duration for all stages. |
120 Seconds |
|
HTG-MINON, PH-MINON, or RH-MINON (Minimum On Time) |
Contains the Min On Duration for all stages. |
120 Seconds |
|
HTG-O, PH-O, or RH-O (Heating Percent Cmd) |
V |
Controls the heating device. The device is commanded from 0% to 100%. |
Display Units: % |
HTG-OUTSTATE, PH-OUTSTATE, or RH-OUTSTATE (State) |
G, V |
Current operational mode of the output controller. |
Set Name: AHU Htg Staged State |
Instant Shutdown |
V |
Contains the indication to the MSC to shut off all outputs instantly. |
|
Limited Max Value |
Defines the proportional valve position or the face and bypass damper position when the module is in the Limited Max Heating state. |
100.0% |
|
Low Limit Process Variable |
Contains the low limit temperature process variable. |
7 °C, 45 °F |
|
Low Limit Setpoint |
Low limit temperature setpoint. |
7 °C, 45 °F |
|
Max Capacity Fraction |
Contains the ratio of the largest stage to the sum of all the stages. |
1.0 |
|
Mode |
Mode requested by State Selection. |
Off Set Name: AHU Htg Staged Out |
|
Output Overridden |
Indicates when the actual output controlled by this output is overridden by a user. |
False |
|
Output Position |
Provides the current Present Value of the output that this controller drives. |
0% |
|
PID Tuning Reset |
Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID. |
Normal Set Name: PID Tuning Reset |
|
PMAC Period |
V |
Period used by the PMAC algorithm portion of the MSC. |
Display Units: Seconds |
Process ID |
Type of process that this output controller is controlling when the mode is Control. |
DA-T Set Name: Process ID |
|
Process Units |
Specifies the units for the PID. For this particular module, °C and °F are the only two valid values. |
°C, °F Set Name: Unit |
|
Process Variable |
Control temperature. Either Zone temperature, discharge air temperature, return air temperature or preheat temperature may be connected to this input. |
13 °C, 55 °F |
|
Proof of Airflow |
Specifies that when set to False or True, the controller operates as normal. When set to Fault, the controller transitions to an instant off state. |
True Set Name: False/True/Fault |
|
Setpoint |
Contains the desired setpoint for the process variable to be controlled to when the mode is Control. |
13 °C, 55 °F |