Reliability (Heating Sequenced Valves with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Table 1. Heating Sequenced Valves with Low Limit Reliability

Input

Behavior When Input Is Not Reliable

OA Temperature

If the requested mode is Low OA Temperature, the output controller changes to Failsoft.

Low Limit Process Variable

If the requested mode is Remain In Control, the output controller changes to Failsoft.