Attributes (Heating FBPD Proportional Valve with Low Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Heating FBPD Proportional Valve with Low Limit modules.

Table 1. Heating FBPD Proportional Valve with Low Limit Attributes

Name

Type 1

Description

Default Value

Compensator Htg Cmd

 

Controls the heating valve. The valve is commanded from 0% to 100%. This output incorporates the Lead Compensator.

0.0

Display Units: %

Damper Percent Cmd

V

Controls the face and bypass damper. The damper is commanded from 0% (full bypass) to 100% (full face).

Display Units: %

Failsoft Value

 

Defines the face and bypass damper position when the module is in the Failsoft state.

100.0%

FBPDSWO-SP (Switchover Setpoint)

 

Contains the switch over setpoint. If the Switchover Process Variable Temperature is greater than the setpoint, the valve is the controlled device. If the Switchover Process Variable Temperature is less than the setpoint, the face and bypass damper is the controlled device.

4 °C, 40 °F

Flush Position

 

Defines the proportional valve position when the module is in the Water Flush state.

100.0%

Heating Control Status

V

Current saturation status of the controller.

Set Name: Control Status

Heating Percent Cmd

V

Controls the heating valve. The valve is commanded from 0% to 100%.

Display Units: %

Heating Ramp Rate

 

Used to determine the time to remain in the Cold Start state (if applicable). During the cold start state, the preheat output is prevent from closing quickly to allow it to come into control without tripping the Low Limit on the unit.

20.0%

HTG-OUTSTATE or PH-OUTSTATE (State)

G, V

Current operational mode of the output controller.

Set Name: AHU Htg w FBPD Valve Out

Limited Max Value

 

Defines the face and bypass damper position when the module is in the Limited Max mode.

100.0%

Low Limit Process Variable

 

Low limit temperature process variable. This input is usually the preheat or discharge air temperature.

7 °C, 45 °F

Low Limit Setpoint

 

Low limit temperature setpoint.

7 °C, 45 °F

Low OA Temperature Diff

 

Contains the differential for the Low OA Temperature function. Once the valve has been opened in the Low OA Temperature mode, the OA Temperature must increase Low OA Temperature Diff more than the Low OA Temperature Setpoint before the valve can close.

0.5 °C, 1 °F

Low OA Temperature Position

 

Defines the proportional valve position or the face and bypass damper position when the module is in the Low OA Temperature state.

100.0%

Low OA Temperature Setpoint

 

Contains the setpoint for the Low OA Temperature function. When the OA Temperature is below this setpoint, the valve opens and the face and bypass damper is set to Low OA Temperature Position.

4 °C, 40 °F

Mode

 

Mode requested by State Selection.

Off

Set Name: AHU Htg Valve Out

Network Switchover

 

Contains the network switch over variable which is used to determine if the valve or the FBPD is the control device.

FBPD

Set Name: FBPD/Valve

OA Temperature

 

Outdoor air temperature.

4 °C, 40 °F

Output Overridden

 

Indicates when the actual output controlled by this output is overridden by a user.

False

Percent Cmd

V

Shows the total system output from 0% to 100%.

Display Units: %

PID Tuning Reset

 

Causes the PID objects to reset their tuning parameters to the default based on the appropriate Process ID.

Normal

Set Name: PID Tuning Reset

Process ID

 

Type of process that this output controller is controlling when the mode is T Control. The following lists the process variables and the correct setting for the Process ID:

Process Variable: Process ID
  • Discharge Air Temperature: DA-T
  • Preheat Air Temperature: DA-T
  • Return Air Temperature: ZN-T
  • Zone Air Temperature: ZN-T
  • Exhaust Air Temperature: ZN-T
  • Zone Air Temp Compensated: ZN-T LC

DA-T

Set Name: Process ID

Process Units

 

Specifies the units for the PID. For this particular module, °C and °F are the only two valid values.

°C, °F

Set Name: Unit

Process Variable

 

Control temperature. Either Zone temperature, discharge air temperature, return air temperature, or preheat temperature may be connected to this input.

13 °C, 55 °F

Pump OnOff

V

Controls the circulating pump.

Set Name: Off/On

Setpoint

 

Desired setpoint for the process variable to be controlled to when the mode is T Control.

13 °C, 55 °F

Switchover Diff

 

Specifies the switch over differential. The Switch T must be this much more than the setpoint before the module may return to valve control.

0.5 °C, 1 °F

Switchover Process Variable

 

Contains the switch over variable which is used to determine if the valve or the FBPD is the control device. The mixed air temperature or the outdoor air temperature are usually connected to this input.

4 °C, 40 °F

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)