Heating & Cooling Control - Heating - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Heating output controllers controls a heating device. Support for two position valves, face and bypass dampers, proportional valves, and staged outputs is included. Support for face and bypass dampers combined with proportional or two position valves is also included. Some of the modules also provide for low limit control.