Reliability (Cooling Proportional Valve with Dehumidification) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

All inputs use their last reliable value while unreliable.

If the outdoor air temperature is unreliable while in the Low OA Temperature mode, the module switches to the Limited Max mode as shown in Table 1.