Primary States (Cooling Proportional Valve) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Sets the Percent Cmd to 0%.

  • Max: The Percent Cmd is set to 100%.

  • Limited Max: Set the Percent Cmd to the Limited Max Value.

  • Hold: Hold the Percent Cmd at the current value.

  • Water Flush: Set the Percent Cmd to Flush Position.

  • Control: Adjust the Percent Cmd to control the Process Variable.

  • Failsoft: Set the Percent Cmd to the Failsoft value.