The following table describes the attributes used by the Single Speed Fan Control modules.
Name |
Type 1 |
Description |
Default Value |
---|---|---|---|
Fan OnOff |
Contains the output command enumeration for information feedback representing the on/off status of the fan. |
Set Name: Off/On |
|
Mode |
Mode requested by State Selection. |
Off Set Name: Off/On |
1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)