Attributes (Parallel Fan Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Parallel Fan Control modules.

Table 1. Parallel Fan Control Attributes

Name

Type

Description

Default Value

Input

 

The input to the pass through module

Off

Set Name: Off/On

Present Value

G, V

The output of the pass through module

Set Name: Off/On