Primary States (Fan Proportional) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Turn the fan off. The Percent Cmd is set to 0% and the Fan OnOff is set to Off.

  • On: Turn the fan on at the appropriate speed. The speed is determined internally based on a span of the Minimum Speed and the max heating or cooling percentage inputs.

  • Max: Turn the fan on at the max heating speed. The Percent Cmd is set to the Max Speed Heating.