Attributes (Fan Proportional) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The following table describes the attributes used by the Fan Proportional modules.

Table 1. Fan Proportional Attributes

Name

Type cku1558008196875.html#cku1558008196875__cconfiguration_mode_gdefault

Description

Default Value

Cooling Percent Cmd

 

Contains the percent cooling, typically connected from the cooling output module. This value is used to span to a fan speed.

 

Fan OnOff

 

Contains the output command enumeration for information feedback representing the on/off status of the fan.

Set Name: Off/On

FAN-OUTSTATE (State)

 

Current operational state of the output controller.

Set Name: Off/On/Max

Heating Percent Cmd

 

Contains the percent cooling, typically connected from the heating output module. Used to span to a fan speed.

 

Max Speed Cooling

 

Contains the output percentage when the Cooling Percent Cmd input is at 100%.

100.0%

Max Speed Heating

 

Contains the output percentage when the Heating Percent Cmd input is at 100%.

100.0%

Minimum Speed

 

Specifies that when commanded to on, this is the minimum value that is output in the Percent Cmd output.

20.0%

Mode

 

Mode requested by State Selection.

Off

Set Name: Off/On/Max

Percent Cmd

 

Output for fan control (0-100%).

Display Units: %

1 C - Configuration Mode Only, G - Default Element (Generated State, if applicable), SC - Simulation and Commissioning Modes Only, V - Calculated Value (Outputs)