Fan Supply Duct Static Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module is designed to use the supply fan to control the supply air duct static pressure. The module has inputs for the desired mode, a ramp rate, pressure, pressure setpoint, and process units. The module is also designed to accept commands from a FSCS. The FSCS input takes precedence over the mode input.