This module is designed to start and stop two fans so they run in a lead lag fashion for an air handler application and two other outputs to control the speed of those fans. The module monitors the two supply fans command, alarm status, and speed to determine whether the lag fan needs to operate. This module is implemented as a control activity.
You can view and modify the modules in this group’s logic.