The application System Selection Trees use the individual modules in this group using the names in the following table.
Module Instance Name |
Applications |
---|---|
2 Pipe Pump Sequencer | |
Cooling Pump Sequencer |
AHU 100% Outdoor Air Dual Duct Applications AHU 100% Outdoor Air Single Duct Applications AHU Multizone (Mixed Air Dual Duct) Applications |
Preheat Pump Sequencer |
AHU 100% Outdoor Air Dual Duct Applications AHU 100% Outdoor Air Single Duct Applications AHU Multizone (Mixed Air Dual Duct) Applications |
Reheat Pump Sequencer |
AHU 100% Outdoor Air Dual Duct Applications AHU 100% Outdoor Air Single Duct Applications AHU Multizone (Mixed Air Dual Duct) Applications |
To see a module's connections and how modules interact with it, view the Connections table.