Device OR - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
This module is responsible for examining two enumeration inputs and provides OR logic where at least one input must be On for the output to be On. The module accepts two Off/On inputs and has a output.