Module Use in Applications (Min OA Fan Variable Capacity Flow Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Min OA Fan Variable Capacity Flow Control Uses in Application System Selection Trees

Module Instance Name

Applications

Variable Capacity Fan Minimum OA Flow Control v50

AHU Mixed Air Single Duct Applications

AHU Mixed Air Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.