Damper Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Damper Control modules provide for outdoor and return economizer dampers control of the process variable at the setpoint. The output controllers also provide for low limit control. The module for Damper Control for UV Cycle 1, 2, or W provide specific sequencing to meet the ASHRAE cycles 1, 2, or W for unit ventilators.