Primary States (VF Primary Min Flow Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04
  • Off: Sets the Percent Cmd to 0%.

  • Max: Sets the output for maximum. The Percent Cmd is set to 100%.

  • Control: Adjusts the output to control the Process Variable to the setpoint. If the Process Variable is reliable, the module controls the output to maintain the process variable at the Setpoint.

  • Hold: Outputs remain at the last value.