Primary States (Tower Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Turn the device off. Set the Output to 0%, set the Alarm to Off, delay off the interlock Command, and set the Command to Off.

  • On: Enable the inputs to start and stop the device.