The Sequenced Output module takes one proportional output and spans it over two proportional outputs. This module accepts as inputs an Input (float) and a Valve 1 Percent Capacity. Based on the input commands, the module outputs two proportional outputs.
You can view and modify the modules in this group’s logic.