Rotation Small - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1

Controller Tool Help

Product name
Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
13.1
Revision date
2019-12-04

The Rotation Small module provides the same logic as the Sequencer 08 module (See the Sequencer 01 through Sequencer 16 section.). The Sequencer module provides multiple stage sequence control. This module is designed to control discrete systems where the relative capacities of the stages are known. This module uses relative capacities to determine which outputs to turn on or off. For example, three boilers with different capacities (x btu, y btu, and z btu) allow for 8 stages of control. The method is based on the split-range control concept and allows multiple stages to be controlled by a single feedback controller, such as a PID. This module should be operated continuously (that is, do not place this module in a hybrid activity because the activity disables all modules associated with a specific state when that state is not active.)

You cannot view and modify this modules in this group’s logic.