Module Use in Applications (Ramp to Command with Limit) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Ramp to Command with Limit Uses in Application System Selection Trees

Module Instance Name

Application

Boiler Pump XX Speed Control (Where XX Is 01-08)

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.