Primary States (Pump Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Turns the device off. The Output is set to 0%, the Alarm is set to Off, and the Device OnOff is delayed off.

  • Control: Enables the Command Input to start and stop the device.

  • Instant Shutdown: Turns the device off immediately. The Output is set to 0%, the Alarm is set to Off, and the Device OnOff is set to Off. This state is used for Emergency Shutdown only and bypasses all timers which may cause dangerous conditions.

  • Interlock Only: Works the same as the Control Mode.