Primary States (Plant Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
  • Off: Turns the device off. The Output is set to 0%, the Alarm is set to Off, the interlock Command is delayed off, and the Command is set to Off.

  • Control: Enables the Command Input to start and stop the interlock and the device.

  • Instant Shutdown: Turns the device off immediately. The Output is set to 0%, the Alarm is set to Off, the interlock Command is off, and the Command is set to Off. This state is used for Emergency Shutdown only and bypasses all timers which may cause dangerous conditions.

  • Interlock Only: Enables the Command Input to start and stop the interlock.