Module Use in Applications (Plant Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Plant Control Uses in Application System Selection Trees

Module Instance Name

Applications

Boiler X Control (Where X Is 1-8)

Central Heating Applications

Chiller X Control (Where X Is 1-8)

Central Cooling Applications

To see a module's connections and how modules interact with it, view the Connections table.