Module Use in Applications (Heat Exchanger with Return Water Control) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Heat Exchanger with Return Water Control Uses in Application System Selection Trees

Module Instance Name

Applications

Heat Exchanger with Return Water Output v51 (Heat Exchanger with Low Limit Output v51)

Central Heating Applications

To see a module's connections and how modules interact with it, view the Connections table.