The application System Selection trees use the module names in the following table.
Module Instance Name | Applications |
---|---|
Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
EA Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
OA Damper Command OR | AHU 100% Outdoor Air Single Duct Applications |
To see a module's connections and how modules interact with it, view the Connections table.