Damper Command OR - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Damper Command OR module provides the ability to OR the inputs to the module and passes the result to the output. This module is implemented as a control activity.

Figure 1. Damper Command OR