Module Use in Applications (Min Flow Control [VAV Dual Duct]) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Min Flow Control (VAV Dual Duct) Uses in Application System Selection Trees
Module Instance Name Applications
Min Flow Control (VAV Dual Duct) VAV Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.