Module Use in Applications (HD Constant Flow Setpoint) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees in the software use the individual modules in this group using the name in the following table.

Table 1. HD Constant Flow Setpoint Uses in Application System Selection Trees

Module Instance Name

Applications

HD Constant Flow Setpoint Control

VAV Dual Duct Applications

VAV Slave Dual Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.