Module Use in Applications (Cascaded Discharge Air Setpoint Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection trees use the individual modules in this group using the names in the following table.

Table 1. Cascaded Discharge Air Setpoint Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Cascaded Discharge Air Setpoint Determination v51

AHU Mixed Air Single Duct Applications

AHU 100% Outdoor Air Single Duct Applications

AHU Rooftop Unit Applications

Box Htg DA Setpoint Reset

VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.