Module Use in Applications (Cascaded DA Setpoint Determination) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The application System Selection Trees use the individual modules in this group using the names in the following table.

Table 1. Cascaded DA Setpoint Determination Uses in Application System Selection Trees

Module Instance Name

Applications

Cascaded DA Setpoint Determination VAV Single Duct Applications
Box Htg Setpoint Reset VAV Single Duct Applications

To see a module's connections and how modules interact with it, view the Connections table.