Cascaded Zone Control - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Cascaded Zone Control output controllers provide a setpoint for another control loop (discharge air temperature or VAV flow control). The output controllers vary the setpoint based on the zone temperature and the appropriate zone heating or cooling setpoint.