Output Control Interface Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
The Output Control Interface Network Outputs are always paired with an Output Control module. These outputs receive a state condition from their paired Output Control module that is captured in the State Selection Table. For example, the EFFZNDPR-MODE Network Output is integrated with the Zone Damper Mode Pass Through Output Control module.

The following table describes the Output Control Interface Network Output modules and lists the applications in which they are used.

Table 1. Output Control Interface Network Outputs Modules

Name

Description

Applications

EFFZNDPR-MODE

Zone Damper Mode CSO - Receives input from the Zone Damper Mode Pass Through Output Control module.

AHU Multizone (Mixed Air Dual Duct) Applications

EFFZNHTGVALVE-MODE

Zone Htg Valve Mode CSO - Receives input from the Zone Damper Mode Pass Through Output Control module.

AHU Multizone (Mixed Air Dual Duct) Applications

EFFZNSTAGEDHTG-MODE

Zone Staged Htg Mode CSO - Receives input from the Zone Damper Mode Pass Through Output Control module.

AHU Multizone (Mixed Air Dual Duct) Applications