For Custom Application creation, generic Network Outputs can be created using the right-click > New process available on the Network Outputs header in the Control View. You have the choice of creating a Boolean, Enum, or Float-based Network Output that can be renamed and integrated into the custom logic. See Adding a Network Output in the Configuring a System section.
The following table describes the generic Network Output modules and lists the applications in which they are used.
Name |
Description |
Applications |
---|---|---|
OUTPUT-BOOLEAN |
CS Output (Boolean) |
Custom Applications |
OUTPUT-ENUM |
CS Output (Enum) |
Custom Applications |
OUTPUT-FLOAT |
CS Output (Float) |
Custom Applications |