Sensor and Setpoint Modules - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 13.1
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
Key Sensor and Setpoint Network Inputs are created during System Selection to allow system-wide logic to easily interface with the local control logic.

Typical examples for sensors include scenarios when the Supervisory System provides Outdoor Air Temperature and Humidity values for all the local devices using Network Inputs. An example use is that a Supervisory device reads an Outdoor Air Temperature sensor from one device and writes its value to the network input of other devices.

Another example is that slave VAV box applications read key values from the master VAV box applications using peer-to-peer references to make sure the zone under control does not have some VAV boxes calling for cooling while others are calling for heating.

The following table describes the Sensor and Setpoint Network Input modules and lists the applications in which they are used.

Note:

If you wish to change the default names used for these modules, you can do so by editing the Object Naming Preferences. See the following topics in the Setting Preferences section for details: Object Naming and Signal Preferences, Setting Default Naming and Signal Preferences, and Preferences - Naming and Signal.

Table 1. Sensor and Setpoint Network Input Modules

Name

Description

Applications

BLDGP-SP

Building Static Pressure Setpoint

BLR-SP

Boiler Setpoint

Central Heating Applications

BLRSTG-SP

Boiler Stage-up Setpoint

Central Heating Applications

CD-OA%

CD OA Percent

CDT-SP

Cold Deck Air Temperature Setpoint

CH-SP

Chiller Setpoint

CHW Coil X Percent Cmd (Where X Is 1-4)

CHW Coil X Percent Cmd

Central Cooling with Optimization Applications

CHWDP-SP

CHW Differential Pressure Setpoint

CHWDT-SP

Differential Temperature Chill Water Setpoint

Central Cooling Applications

CLGOATLOCKOUT-SP

OA Cooling Enable Setpoint

CLGUNOCC-SP

Night Cooling Setpoint

All Air Handling Unit Applications

CP X Runtime Reset (Where X is 1 or 2) CP 1 Runtime Reset, CP 2 Runtime Reset

All Air Handling Unit Applications

CTSTG-SP

CT StageUp Setpoint

Central Cooling Applications

CT-MINOFF

Cooling Tower Minimum Off Time

Central Cooling with Optimization Applications

CT-MINON

Cooling Tower Minimum On Time

Central Cooling with Optimization Applications

CW-SP

Condenser Water Setpoint

CWDP-SP

CW Differential Pressure Setpoint

Central Cooling with Optimization Applications

CWDT-SP

CW Differential Temp Setpoint

Central Cooling with Optimization Applications

CW VFD Ramp Time

CW VFD Ramp Time

Central Cooling with Optimization Applications

DAP-SP

Duct Static Pressure Setpoint

DATLL-SP

Discharge Air Low Limit Setpoint

DAT-SP

Discharge Air Temperature Setpoint

DCPLF-SP

Decouple Loop Flow Setpoint

Central Cooling with Optimization Applications

DEHUM-SP

Dehumidification Setpoint NI

EAT-SP

Exhaust Air Temperature Setpoint

AHU 100% Outdoor Air Single Duct Applications

EFSTG-SP

Exhaust Fan Stageup Setpoint

AHU 100% Outdoor Air Single Duct Applications

FAN-RESET

Fan Alarm Reset

FBPD-SWO

Network Switchover

FLOW-DIFF

Flow Differential Setpoint

FLOW-LL

Airflow Low Limit

FLUSHPOS

Flush Position

FROST-DIFF

Frost Protect Differential

Central Heating Applications

FROST-SPX (Where X Is 1-2)

Frost Protect OA Setpoint X

Central Heating Applications

FSCS-EF

FSCS Exhaust Fan

FSCS-RF

FSCS Return Fan

FSCS-RLF

FSCS Relief Fan

FSCS-SF

FSCS Supply Fan

HCP X Runtime Reset (Where X is 1 or 2) HCP 1 Runtime Reset, HCP 2 Runtime Reset

HD-OA%

HD OA Percent

HDT-SP

Hot Deck Air Temperature Setpoint

HTGOATLOCKOUT-SP

OA Heating Enable Setpoint

HTGUNOCC-SP

Night Heating Setpoint

All Air Handling Unit Applications

HUM-SP

Humidification Setpoint NI

HWDP-SP

HW Differential Pressure Setpoint

Central Heating Applications

HWFLOW-SP

HW Min Flow Setpoint

Central Heating Applications

HWLO-SP

HW Low Setpoint

Central Heating Applications

HWTHI-SP

Hot Water Supply Temperature High Reset Temperature Output Range High

Central Heating Applications

HWTLO-SP

Hot Water Supply Temperature Low Reset Temperature Output Range Low

Central Heating Applications

HWT-OARSTA

Hot Water Supply Temperature Setpoint Reset Input Range Low

Central Heating Applications

HWT-OARSTB

Hot Water Supply Temperature Setpoint Reset Input Range High

Central Heating Applications

HXSTG-SP

Heat Exchanger Stage-up Setpoint

Central Heating Applications

ISOVLV-RT

Chlr IsoVlv Ramp Time

Central Cooling with Optimization Applications

MAT-SP

MA Temperature Setpoint

Unit Ventilator Applications

MOADPOS-SP

Min OA Damper Position

MOAFLOW-SP

Min OA Flow Setpoint

MSTCDFLOW-OUTSTATE

Master CD Constant Flow Setpoint Control

VAV Slave Dual Duct Applications

MSTCDFLOW-OUTSTATE

Master CD Flow Setpoint Control

VAV Slave Dual Duct Applications

MSTHDFLOW-OUTSTATE

Master HD Flow Setpoint Control

VAV Slave Dual Duct Applications

MSTRCDFLOW-PERCENT

Master CD Flow Percent

VAV Slave Dual Duct Applications

MSTRFAN-C

Master Fan Command

VAV Slave Single Duct Applications

MSTRFAN-O

Master Fan Output

VAV Slave Single Duct Applications

MSTRFLOW-PERCENT

Master Supply Flow Percent

VAV Slave Single Duct Applications

MSTRFLOW-S

Master Flow Setpoint Status

VAV Slave Single Duct Applications

MSTRHDFLOW-PERCENT

Master HD Flow Percent

VAV Slave Dual Duct Applications

MSTRHTG-1C

Master Heating Stage 1 Cmd

VAV Slave Single Duct Applications

MSTRHTG-2C

Master Heating Stage 2 Cmd

VAV Slave Single Duct Applications

MSTRHTG-3C

Master Heating Stage 3 Cmd

VAV Slave Single Duct Applications

MSTRHTG-C

Master Heating Command

VAV Slave Single Duct Applications

MSTRHTG-O

Master Heating Output

VAV Slave Single Duct Applications

MSTRSUPHTG- CMSTRSUPHTG1-C

Master Supp Heating Command

Master Supp Heating Stage 1 Cmd

MSTRSUPHTG-O

Master Supp Heating Output

MSTRZN-CO2

Master Zone CO2

VAV Slave Single Duct Applications

OAD-MINPOS

OA Damper Minimum Position

OA-H

Outdoor Air Humidity

OALT-SP

OA Low Limit SP

Central Heating Applications

OA-PERCENT

OA Percent

OA-T

Outdoor Air Temperature

All Applications (except VAV Slave Applications)

OCCFLOW-DIFF

Occupied Flow Differential Setpoint

PCHWP VFD Ramp Time

PCHWP VFD Ramp Time

Central Cooling with Optimization Applications

PHP X Runtime Reset (Where X is 1 or 2) PHP 1 Runtime Reset, PHP 2 Runtime Reset

All Air Handling Unit Applications

PHP-ROT Preheat Pump Rotate Now

All Air Handling Unit Applications

Pump Delay

Pump Delay

Central Cooling with Optimization Applications

RAT-SP

Return Air Temperature Setpoint

RFSTG-SP

Return Fan Stageup Setpoint

AHU Mixed Air Single Duct Applications

Relief Fan Stageup Setpoint

AHU Mixed Air Single Duct Applications

RHP X Runtime Reset (Where X is 1 or 2) RHP 1 Runtime Reset, RHP 2 Runtime Reset

All Air Handling Unit Applications

RHP-ROT Reheat Pump Rotate Now

All Air Handling Unit Applications

SA-T

Supply Air Temperature

VAV Single Duct Applications

SCHWPSTG-SP

Secondary Chill Water Stageup Setpoint

Central Cooling Applications

SCHWP VFD Ramp Time

SCHWP VFD Ramp Time

Central Cooling with Optimization Applications

SFSTG-SP

Supply Fan Stageup Setpoint

SHWPSTG-SP

Stageup Setpoint

Central Heating Applications

SLH-SP

Sideloop Humidity Setpoint

Sideloop Applications

SLP-SP

Sideloop Pressure Setpoint

Sideloop Applications

SLT-SP

Sideloop Temperature Setpoint

Sideloop Applications

STAGE-CAP

Stage Capacity

Stage Capacity (%FLA)

Stage Capacity (AMPS)

STMP-SP

Setpoint

Central Heating Applications

UNIT-RESET

Unit Reset

All Air Handling Unit Applications

UNOCCFLOW-DIFF

Unoccupied Flow Differential Setpoint

ZN-H

Zone Humidity

ZN-T

Zone Temperature

ZNT-SP

Common Setpoint

Zone Temperature Setpoint

ZNX-SP

Zone X Common Setpoint (where X is 1-8)

AHU Multizone (Mixed Air Dual Duct) Applications

Zone X Temperature Setpoint (where X is 1-8)

Central Heating Applications

ZONE-DIFF

Zone Differential

Central Heating Applications